2004-10-28 1:01 AM
2004-10-26 7:55 PM
I have a tabel with text strings.
Like: Name, ETX Version, ETX etc. Now i want to read each text seperate. So 1 pointer for the text string and 1 pointer for each letter of th string. HOW? Assembler can only handle one pointer! ld a(text,x) Write A to sci, till ETX I,ve tried to made text a pointer, but it doesn't work. Problem with byte-word value. Anybody made a 2 dimensional pointer? Or have somebody a better idea?2004-10-27 4:39 AM
Moppie,
if you use assembler, take a look to the indirect addressing... If you want 2 dimensional data access, you have to define a pointers' table (the address of the first character of a string) and use the X register to displace from the first character. To access the 2nd char of the 3rd string you can write the following: ; put this declaration in the ram segment ptr DS.w ; this declaration in in the rom segment text DS.w ; addresses of the first character of each string ; select the 3rd string LD X,#3 SLL X LD A,(text,X) LD ptr,A LD A,({text+1},X) LD {ptr+1},A ; select the 2nd character LD X,#2 LD A,([ptr.w],X) ; Do whatever you want ... I hope I was clear... EtaPhi2004-10-27 8:08 PM
Thanks for you're reply.
I've copied you're code and it works fine, thanks. But, i changed the DS.W to DC.W in the ROM segment. I get errors from the compiler Fatal 999: Cannot mix Storage and Static definitions in same segment! 'S->D' In the ROM segment i only use DC.B/W. What is the big difference between these?2004-10-28 1:01 AM
I am sorry for the mistake, Moppie...
When I sketched the data structure I did not care too much to the DS (define storage, i.e. bytes readable and writeable) and DC (define constant) directives... This explains the assembler error: the rom can not contain variables! BTW, my example is useful when there are static strings whose lenght is not the same. These data object are typically expressed in C as: #define MAX_STRINGS 10 const char *text[MAX_STRINGS]; If you want to reduce the clock cycles (at the price of some memory waste), you can use the following C data structure: #define MAX_STRINGS 10 #define MAX_STR_LEN 8 const char text[MAX_STRINGS][MAX_STR_LEN]; The big difference is that in the latter you can use an expression to compute the position of the character to read. Let's say you want read text[3][2], as in my first example. here is what I'd write: LD X,#3 LD A,#MAX_STR_LEN MUL X,A ADD A,#2 LD X,A LD A,(text,X) Pls, note that some cycles can be saved if MUL X,A can be replaced by a logical shift to left (i.e. MAX_STR_LEN is a power of 2). Regards, EtaPhiWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.