2008-10-06 3:31 AM
STR912FW44: Data abort after 32k flash boundary (ADR 0x8000 and higher)
2011-05-17 12:56 AM
Hi guys,
I am writing a C low level startup sequence for the STR912FW44. After the routine has finished, the code then tries to read flash memory past a 32k ''boundary'' (address 0x8000 and higher), e.g. address 0xa444, and a data abort exception is thrown. The STR912FW44 has 512k flash mapped to bank 0 and 32k flash is mapped to bank 1. I am able to successfully program a 41k application into flash. Can anyone give me a hint of what I might be missing or doing wrong? Thanks! Pieter Here is my C initialisation code: void LowLevelInit(void) { /* ''Buffered'' is defined in ''91xconf.h'' */ #ifdef Buffered __asm__ __volatile__( ''mrc p15, 0, r0, c1, c0, 0 \n\t'' /* Read CP15 c1, Control Register */ ''orr r0, r0, #0x8 \n\t'' /* Enable BIU write buffer on AMBA AHB */ ''mcr p15, 0, r0, c1, c0, 0 \n\t'' /* Write CP15 c1, Control Register */ : : : ''r0''); #endif /* * Set bits 17 (Data TCM order bit) and bit 18 (Instruction TCM order bit) * in the Configuration Control Register. */ __asm__ __volatile__( ''mov r0, #0x60000 \n\t'' ''mcr p15, 1, r0, c15, c1, 0 \n\t'' : : : ''r0''); /* * Map Flash Bank 0 at address 0x0 and Bank 1 at address 0x80000, * when the bank 0 is the boot bank, then enable the Bank 1. */ FMI->BBADR = 0x00000000>>2; /* Set Boot bank base address to 0x00000000 */ FMI->BBSR = 4; /* Set Boot bank size to 512KB */ FMI->NBBADR = 0x00080000>>2; /* Set Non boot bank base address to 0x00080000 */ FMI->NBBSR = 2; /* Set Non boot bank size to 32KB */ FMI->CR = 0x18; /* Enable Flash Boot Bank and Non Boot Bank */ /* Enable SRAM */ SCU->SCR0 = 0x187 | (2 << 3); /* Set System configuration register to 96K SRAM size */ }2011-05-17 12:56 AM
Hi pieter,
Here my init function, which do exactely what you are looking for: I m using the Bank0 for startup-program and the bank1 for emulate EEPROM and keep some data. Both work correctly. I use the lib. from ST. You can take a look also on the other part of the code (commented #if 0), this code works, and don't use the ST lib. Regards. Damien FMI_BankRemapConfig (0x04,0x02,0x00000000, 0x00080000); //Arg 1 -> 0x4: Boot bank size 512KBytes. //Arg 2 -> 0x2: Non Boot bank size 32KBytes. //Arg 3 -> Mapping address boot bank //Arg 4 -> Mapping address NON boot bank /* Turn ON clock*/ SCU_FMICLKDivisorConfig(SCU_FMICLK_Div1); //never put FMI in reset here, or will crash SCU_AHBPeriphClockConfig(__FMI, ENABLE); SCU_AHBPeriphReset(__FMI, DISABLE); FMI_Config(FMI_READ_WAIT_STATE_2, FMI_WRITE_WAIT_STATE_0, FMI_PWD_ENABLE,FMI_LVD_ENABLE, FMI_FREQ_HIGH); #if 0 //previous code, from the STR912 GCC port from Richard Berry, FreeRTOS corp. // For info only FMI->BBSR = 4; FMI->NBBSR = 2; FMI->BBADR = (0 >> 2); FMI->NBBADR = (0x80000 >> 2); FMI->CR |= 0x18; FMI->CR &= FMI_WRITE_WAIT_STATE_0; *(vu16 *)FMI_BANK_1 = 0x60; /* need 3 read wait states if operating @ 96Mhz */ *(vu16 *)(FMI_BANK_1 | FMI_READ_WAIT_STATE_3 | FMI_PWD_ENABLE | FMI_LVD_ENABLE | FMI_FREQ_HIGH) = 0x03; #endif2011-05-17 12:56 AM
Hi Damien,
Thanks for the help! It turns out that if DEBUG is defined in ''91xconf.h'' (or in my Makefile), the peripheral registers are declared as ''extern'' in ''91x_map.h'' and initialised to correct values in the function ''debug()'' in ''91x_lib.c''. I did not call ''debug()'' first and my lowlevel C initialisation function accessed random values in stead of correct registers. Regards, PieterWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.