2007-01-03 8:45 PM
2006-12-21 9:13 AM
Hi All!
Is it possible to update whole Bank 0 memory via bootloading program previously programmed to Bank 1? Is it possible to make such organization? If No, why? I think not, but I just want to be sure. Thanks in advance. Hristo.2006-12-22 1:41 AM
Hi,
could you please precise which STR7x product are you using? Thanks,2006-12-26 9:34 PM
I'm using STR711FR2 microcontroller.
2007-01-03 8:45 PM
Remember, it is not possible to boot directly from bank 1. So you need some piece of code stored also in bank 0. I think... you can use bootloader stored in bank 0 that will copy itself into RAM, then erase flash bank 0, and finally write bank 0 with new content...
JozefWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.