2007-10-22 11:51 PM
STR73x Reference manual Revision History
2007-10-22 11:51 PM
This thread is reserved for STMicroelectronics, PLEASE DO NOT REPLY.
Dear, New revision ofhttp://STR73x Reference manual
Rev2 is available for download from the web site; Here below, changes compared to the last revision Rev1; + Updated Section 14.3.10:''Pulse width modulation mode''- Added period formula when OCBR> OCAR - Updated period formula when OCBR and OCAR are loaded with FFFCh. + Modified Section 6.1.2:''Alternate function I/O (AF)''- For alternate function inputs, the port must be configured in Input mode and the input pin must be driven externally. + Added Section 11.3.3:''RTC flag assertion''- Added Note: If RTC interrupts are used during Run, Slow, WFI or LPWFI modes the RTC clock must be at least 4 times slower than MCLK clock. + Modified Section 11.4.3:''RTC Prescaler Load Register High (RTC_PRLH)''- Bits 3:0 = PRL[19:16]: These bits are used to define the counter clock frequency according to the following formula: fTR_CLK = fRTC/64/2 ; if PRL[19:0] =0 fTR_CLK = fRTC/64/(PRL[19:0]+1) ; if PRL[19:0] > 0 + Updated Section 11.4.4:''RTC Prescaler Load Register Low (RTC_PRLL)''- Bits 15:0 = PRL[15:0]: These bits are used to define the counter clock frequency according to the following formula: fTR_CLK = fRTC/64/2 ; if PRL[19:0] =0 fTR_CLK = fRTC/64/(PRL[19:0]+1) ; if PRL[19:0] > 0 - Added note: The reset value sets the TR_CLK signal period to 1 sec for an input clock of 32 kHz. + Updated Section 18.2.5:''Start-up status''- The MSTR bit must be set high and then the BSPI must be enabled. + Updated Section 19.4.6:''UART control register (UARTn_SR)''- RxBufFull changed to RxBufNotEmpty. + Updated Section 17.4:''Interrupts''- SCLFAL signal removed from figure 62:''Event flags and interrupt generation''+ Added Section 22.1.1:''JTAG ID code''Best Regards ;)We’re moving the ST Community to a new platform to give you a better and more reliable community experience.