2008-09-08 12:22 AM
2007-09-09 11:45 AM
I have over 100K ported and performing final testing but have discovered some problems with the EIC Interrupts.
Interrupts are occurring but it appears that some extra ones are also occurring. This is happing on both external interrupts and interrupts generated by the timers. Any one else seen this? Have any suggestion? Anyone even using this derivation? It seems like this group is not very proactive or the ST ARM's are not being used. I'm using the Keil compiler.2007-09-21 2:37 AM
we didn't seen this problem. could you provide us more infomations about your hardware and software, timer configuration .. what are the interrupt used in application?
2008-09-08 12:22 AM
Hi !
Did you ensure that you erase all necessary flags for that specific interrupt ? e.g. Timer 0 has two flags. one which informs you about the overflow (or capture, or ...) one which informs you that the interrupt is (still) pending clear both in the correct order and that shall workWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.