2008-09-09 11:07 PM
2008-09-09 9:14 PM
Hello,
I'm working with : STR710 IAR 4.42A Maigcrator Program->Flash The Debugger hangs in _segment_init. Any ideas to debug? Thanks, Steffen2008-09-09 11:07 PM
Wow, it seems I'have found the reason.
I need an extra output file (elf). Therefore I switch the option Linker-Extra Output File to elf. Unfortunately, the FlashLoader needs the sim (Simple Format)- File. Thus, you have to link first with Simple Format, then with the wished Extra-Format. Sounds illogical for me, but it works now. regards, SteffenWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.