2007-11-16 1:45 AM
2007-09-25 4:18 PM
Hello,
I previously posted about the problem getting the STR712 code to execute. That problem was solved when I re-installed RIDE and RFlasher. I must have had something configured that I didn't know about, despite the number of times I checked all the applicable options. At any rate, I'm developing the STR712F2 with Eclipse as my IDE. I have the gnuarm toolchain: gcc version 4.1.1 and binutils 2.1.7. As evidenced by my previous troubles, I have no idea what I'm doing. I was previously using the LPC2106. It was GREAT because I could step through the oodles of tutorials and set-up help that was out there (Jim Lynch is my hero). Unfortunately, we needed four serial ports, so we moved over to the STR712, which is far more capable. I thought it would be a pretty smooth transition, but apparently I was way off with that estimation. I've downloaded sample projects for all sorts of development environments. Many of them even use the gnuarm toolchain, but none of them runs properly when I try and set them up in Eclipse. I CAN get the samples from the ST site to compile and run fine with the RIDE environment; I just don't like their IDE, and to exacerbate things I can't figure out how to add source files to keep my main.c from getting really huge. I know my issue is rooted in the boot sequence for the chip, and with the memory map. All the examples I've found are configured for debugging, so they all run in RAM. I have two demo boards with the boot pin pulled low, so I need to program the chip to run in flash. I've tried altering the linker scripts, writing my own makefile, and all sorts of other stuff, but nothing has worked. I might as well be performing open-heart surgery, since I don't know what to look for or where to start. Does anyone have any basic suggestions about where to start? I've read all the appnotes from ST five times over, and they don't seem to trigger any thoughts in my mind, and I've been searching the internet for four days without much success. Does anyone know if there's a sample project out there with the basic files, makefile, etc all in once place? That would be perfect. Otherwise, any other tips would be greatly appreciated. Matt2007-11-16 1:45 AM
Hi Matt,
maybe you have already solved your problem, and maybe I've not understand very well what you are looking for. I post here an example from Mr Lynch tutorial and I revisited the makefile to work with the project file and ARM toolchain (Eclipse-GNU ARM toolchain-OpenOCD-STR7xx). This project just increments two variables. Is this enough? Marco ________________ Attachments : Str7test.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtQU&d=%2Fa%2F0X0000000aPr%2FutKUTv96fhQ1IpT81DIyKaX7caQkBF0aWGcGFt4Hdjk&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.