2008-11-20 10:22 PM
STR710. I2C. Library version 3.1. Question about I2C_FlagStatus()
2008-11-20 10:22 PM
Hi all,
I have a one question about the INDIRECT access in this function. As you can find for example in: http://www.cplusplus.com/reference/clibrary/cstdarg/va_start.html ''A function that executes va_start, shall also execute va_end before it returns.'' But in the library function from ST there are no such calling. Is it a problem? Can it cause memory leaks or somethimg bad else? Please do not propose to use the new library since the project my almost finished... :) I list the part code from library: FlagStatus I2C_FlagStatus (I2C_TypeDef *I2Cx, RegisterAccess Access, I2C_Flags Flag, ...) { u32 Tmp=0; if (Access == DIRECT) /* Store in Tmp variable the register where is located the flag */ Tmp = I2C_GetStatus(I2Cx)&Flag; else { va_list list; /* Get the fourth register */ va_start(list,Flag); Tmp = va_arg(list,u32); Tmp&=Flag; } /* Return the Flag NewState */ return Tmp != 0 ? SET : RESET; }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.