2008-11-11 2:49 PM
2008-11-11 2:49 PM
I hava designed a product with str710,but the can always crashed. Baud rate is 100K ,about 2 hours start error. It can send ok,but the other mcu dosn't received. I use the ST firmware. It is
u32 CAN_SendMessage(u32 msgobj, canmsg* pCanMsg) { while (CAN->sMsgObj[0].CRR & CAN_CRR_BUSY); /* if (CAN->sMsgObj[0].COMR & CAN_CRQ_BUSY) */ /* return 0; // message interface 0 not free */ CAN->SR &= ~CAN_SR_TXOK; /* read the Arbitration and Message Control */ CAN->sMsgObj[0].CMR = CAN_CMR_ARB | CAN_CMR_CONTROL; CAN->sMsgObj[0].CRR = 1 + msgobj; while (CAN->sMsgObj[0].CRR & CAN_CRR_BUSY); /* update the contents needed for transmission */ CAN->sMsgObj[0].CMR = CAN_CMR_WRRD | CAN_CMR_ARB | CAN_CMR_CONTROL | CAN_CMR_DATAA | CAN_CMR_DATAB; if ((CAN->sMsgObj[0].A2R & CAN_A2R_XTD) == 0) { /* standard ID */ CAN->sMsgObj[0].A1R = 0; CAN->sMsgObj[0].A2R = (CAN->sMsgObj[0].A2R & 0xE000) | STD_FIXED_ID_ARB(pCanMsg->Id); } else { // extended ID CAN->sMsgObj[0].A1R = EXT_FIXED_ID_ARB_L(pCanMsg->Id); CAN->sMsgObj[0].A2R = (CAN->sMsgObj[0].A2R & 0xE000) | EXT_FIXED_ID_ARB_H(pCanMsg->Id); } CAN->sMsgObj[0].MCR = (CAN->sMsgObj[0].MCR & 0xFEF0) | CAN_MCR_NEWDAT | CAN_MCR_TXRQST | pCanMsg->Dlc; CAN->sMsgObj[0].DA1R = ((u16)pCanMsg->Data[1]<Data[0]; CAN->sMsgObj[0].DA2R = ((u16)pCanMsg->Data[3]<Data[2]; CAN->sMsgObj[0].DB1R = ((u16)pCanMsg->Data[5]<Data[4]; CAN->sMsgObj[0].DB2R = ((u16)pCanMsg->Data[7]<Data[6]; CAN->sMsgObj[0].CRR = 1 + msgobj; //////////////////////// CAN_SetRxMsgObj(CAN_RX_MSGOBJ, CAN_STD_ID, 0, CAN_LAST_STD_ID, TRUE); ////////////////////// return 1; } Please help me!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.