2007-08-19 11:38 PM
2007-06-16 12:22 AM
I want to use the Timeout feature of the UART.
When i enable the timeout interrupt for the UART0, i find that the timeout flag is always set in the status register of the UART. This causes the UART0 interrupt to be called repeatedly. How to overcome this problem? The UART0 initialisation routine is pasted below: UART_Init(UART0); GPIO_Config(GPIO0, PIN(8),GPIO_IN_TRI_CMOS); GPIO_Config(GPIO0, PIN(9),GPIO_AF_PP); UART_FifoConfig(UART0, DISABLE); UART_FifoReset(UART0, UART_TxFIFO); UART_FifoReset(UART0, UART_RxFIFO); UART_LoopBackConfig(UART0, DISABLE); UART_Config(UART0,19200,UART_NO_PARITY,UART_1_StopBits,UARTM_8D); UART_RxConfig(UART0, ENABLE); UART_TimeOutPeriodConfig(UART0, UART0Timeout_Period); UART_ItConfig(UART0, (UART_RxBufFull | UART_TimeOutIdle), ENABLE); VectSet(IRQ_UART0,UART0_IRQHandler); EIC_IRQChannelPriorityConfig((IRQChannel_TypeDef)IRQ_UART0, 3); EIC_IRQChannelConfig((IRQChannel_TypeDef)UART0_IRQChannel, ENABLE); UART_OnOffConfig(UART0, ENABLE);2007-06-18 11:43 PM
This is normal behavior. When servicing the interrupt, you need to reload the timeout timer by doing one of the following (see manual):
The UART contains an 8-bit timeout counter. This reloads from UARTn_TOR whenever one or more of the following is true - UARTn_RxBBUFR is read - The UART starts to receive a character - UARTn_TOR is written to Regards, - mike2007-08-19 11:38 PM
you don't mention whic processor you are using...
We had problems with the STR730 because there is a mistake in the C library where the TOR address is not specfied correctly. Make sure you have the latest library update and check that 73x_map.h has: ... vuc16 SR; /*Status Register*/ u16 EMPTY6; u16 EMPTY7; u16 EMPTY8; vu16 TOR; /*Timeout Register*/ ... in it (note the 3 empty definitions, the faulty library only has 1) hope this helps PhilipJWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.