2003-08-04 11:44 PM
2011-05-17 2:34 AM
We are using ST92F150.
Can you provide to me a software example how to enter and leave Stop Mode? Thanks2011-05-17 2:34 AM
Have a look to the attached project.
2011-05-17 2:34 AM
Yes these extra instructions generated can cause problem.
They can be removed by increasing the level of optimization.2011-05-17 2:34 AM
Thanks Romain.
I would be very grateful if you coul help me to understand why I don't enter Stop mode. Here attached the Low_power() function and other definitions. During normal functioning, ADC interrupt and STIM interrupt are working. I'm not able to enter stop mode (STA_DBG always equal to 3). I'm not interested in manage wake-up interrupt, I only need to wake up and restart. Do you see an evident error? Thanks a lot2011-05-17 2:34 AM
In ST92F150, it's written: << to enter STOP Mode, write the sequence 1,0,1 to Stop bit with three consecutive write operations. >>
But the instructions: WU_CTLR |= WUm_stop; WU_CTLR &= ~WUm_stop; WU_CTLR |= WUm_stop; in the .lis file, are assemblied in this way: or @WU_CTLR,#4 ld r0,@WU_CTLR ld @WU_CTLR,r0 and @WU_CTLR,#251 ld r0,@WU_CTLR ld @WU_CTLR,r0 or @WU_CTLR,#4 ld r0,@WU_CTLR ld @WU_CTLR,r0 Having not consecutive 3 write instructions could be a problem ? Thanks a lot2011-05-17 2:34 AM
Thanks.
I already tried with optimization compilation and now works fine!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.