2013-04-24 7:11 AM
Hi together,
I'm writing a application for a STM8S207C8 (64k flash).Currently my code needs 50kB of the flash, what means that the ''magic'' address 0xFFFF is crossed. Therefore I use the compiler option ''+modsl'' (recommended by the compiler manual). This configuration works properly. Now I would like to use the power-on self-test functionality from the ST self-test library. Therefore I created the needed sections in linker file and mapped the call of ''STL_StartUp'' at my reset interrupt vector (as recommended by AN3181, corresponding to the ST self-test library). The bad fact is that with this new configuration I get the following linker error:#error clnk Debug_Standard\sey-redesign.lkf:92 Debug_Standard\stm8s_stl_startup.o: section boundary crossing (.text:00c9) f__stext
I looked for this error code in the STM8 forum but I couldn't find a answer that would help me.
I only found the hint to note the chapter ''Memory Models for code larger than 64K'' in the compiler manual.
It recommends to use the compiler option ''+modsl''. This option I've already used.
Additionally I found the hint to avoid the compiler options ''-gnc'' and ''+nocross''. These options were not used in my application.
Do anyone of you have another idea how to avoid this linker error?
Thanks, Stefan.
I use following environment:
IDE: ST Visual Develop (v4.3.1)
Compiler: COSMIC CXSTM8 (v4.3.7)
Content of the used linker file:
# LINK COMMAND FILE AUTOMATICALLY GENERATED BY STVD:
# * TOTALLY IF AUTO MODE IS ENABLED
# * ONLY INSIDE MARKERS IN SEMI-AUTO MODE
#
# CHOOSE THE CUSTOM MODE IN STVD IN ORDER TO HAVE FULL CONTROL OVER THIS FILE.
#
# Sections delimited by <
BEGIN
...> and <
END
...> markers are reserved for
# STVD: DO NOT MODIFY INSIDE.
#
# Manual modifications are allowed OUTSIDE these sections, WHEN STVD AUTO MODE
# IS DISABLED.
#
# CAUTION:
# * Changing from Custom to Semi-Auto mode removes modifications in
# STVD-reserved sections
# * Changing to Auto mode removes all modifications.
#
# In Semi-Auto mode, you are allowed to remove <
BEGIN
...> and <
END
...> markers
# in order to gain control over the concerned sections. As a consequence any
# modification from the STVD graphical interface concerning this section will be
# ignored.
#
# Please refer to Cosmic User Manuals before any modification.
# Note that errors in editing this file may have unpredictable results when
# running STVD.
# Segment configuration - section reserved for STVD
#<
BEGIN
SEGMENT_CONF>
# Segment Code,Constants:
+seg .const -b 0x9080 -m 0xd980 -n .const -it -ck
+seg .FLASH_CONST -a .const -n .FLASH_CONST
+seg .FLASH_CODE -a .FLASH_CONST -n .FLASH_CODE
+seg .text -a .FLASH_CODE -n .text -ck
+seg .cksum -a .text -n .cksum -ik
# Segment lcDSL flash data:
+seg .lcDSL_flash -b 0x16a00 -m 0x1600 -n .lcDSL_flash -ck
# Segment Eeprom Encoder Settings:
+seg .eep_enc_sets -b 0x4000 -m 0x100 -n .eep_enc_sets
# Segment Eeprom Factory Settings:
+seg .eep_fact_sets -b 0x4100 -m 0x100 -n .eep_fact_sets
# Segment Eeprom #1:
+seg .eeprom -b 0x4200 -m 0x2fe -n .eeprom
# Segment Eeprom Bootloader:
+seg .eep_boot -b 0x44fe -m 0x2 -n .eep_boot
# Segment Eeprom lcDSL:
+seg .eep_lcDSL -b 0x4500 -m 0x100 -n .eep_lcDSL
# Segment Zero Page:
+seg .bsct -b 0x0 -m 0x100 -n .bsct
+seg .ubsct -a .bsct -n .ubsct
+seg .bit -a .ubsct -n .bit -id
+seg .share -a .bit -n .share -is
# Segment Ram:
+seg .data -b 0x200 -m 0xc01 -n .data
+seg .bss -a .data -n .bss
+seg .FLASH_CODE -a .bss -n .FLASH_CODE -a .bss -n boot_RAM -ic
# Segment Class B:
+seg .RUN_TIME_BUF -b 0x100 -m 0x100 -n .RUN_TIME_BUF -m 0x10
+seg .CLASS_B -a .RUN_TIME_BUF -n .CLASS_B -a .RUN_TIME_BUF -m 0x78
+seg .CLASS_B_REV -a .CLASS_B -n .CLASS_B_REV -a .CLASS_B -m 0x78
# Segment Stack Bottom:
+seg .STACK_BOTTOM -b 0xd00 -m 0x100 -n .STACK_BOTTOM
#<
END
SEGMENT_CONF>
# Startup file - section reserved for STVD
#<
BEGIN
STARTUP_FILE>
crtsi.sm8
#<
END
STARTUP_FILE>
# Object files list - section reserved for STVD
#<
BEGIN
OBJECT_FILES>
Debug_Standard\adc.o
Debug_Standard\commands.o
Debug_Standard\eeprom.o
Debug_Standard\error.o
Debug_Standard\hiperface.o
Debug_Standard\init.o
Debug_Standard\lcdsl.o
Debug_Standard\main.o
Debug_Standard\pcbtest.o
Debug_Standard\position.o
Debug_Standard\stm8s_it.o
Debug_Standard\util.o
Debug_Standard\_block_cksumo
Debug_Standard\_classb_cksumo
Debug_Standard\stm8s_stl_clockstart.o
Debug_Standard\stm8s_stl_cpustart_csmc.o
Debug_Standard\stm8s_stl_crc16run.o
Debug_Standard\stm8s_stl_fullram_csmc.o
Debug_Standard\stm8s_stl_main.o
Debug_Standard\stm8s_stl_startup.o
Debug_Standard\stm8s_adc2.o
Debug_Standard\stm8s_awu.o
Debug_Standard\stm8s_beep.o
Debug_Standard\stm8s_clk.o
Debug_Standard\stm8s_exti.o
Debug_Standard\stm8s_flash.o
Debug_Standard\stm8s_gpio.o
Debug_Standard\stm8s_i2c.o
Debug_Standard\stm8s_itc.o
Debug_Standard\stm8s_iwdg.o
Debug_Standard\stm8s_rst.o
Debug_Standard\stm8s_spi.o
Debug_Standard\stm8s_tim1.o
Debug_Standard\stm8s_tim2.o
Debug_Standard\stm8s_tim3.o
Debug_Standard\stm8s_tim4.o
Debug_Standard\stm8s_uart1.o
Debug_Standard\stm8s_uart3.o
Debug_Standard\stm8s_wwdg.o
#<
END
OBJECT_FILES>
# Library list - section reserved for STVD
#<
BEGIN
LIBRARY_FILES>
libisl.sm8
libm.sm8
#<
END
LIBRARY_FILES>
# Interrupt vectors file - section reserved for STVD
#<
BEGIN
VECTOR_FILE>
+seg .const -b 0x9000 -k
Debug_Standard\stm8s_interrupt_vector.o
#<
END
VECTOR_FILE>
# Defines - section reserved for STVD
#<
BEGIN
DEFINED_VARIABLES>
+def __endzp=@.ubsct # end of uninitialized zpage
+def __memory=@.bss # end of bss segment
+def __startmem=@.STACK_BOTTOM
+def __endmem=0x13ff
+def __stack=0x17ff
#<
END
DEFINED_VARIABLES>
#stm8-linker-section-boundary
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.