Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am trying to implement simple spi communication between 2 stm8s. Sending 0x04( address of pin2) and passing the received data as argument to GPIO high .Slave code is txe is not becoming 1 and program stuck there.

I am trying to implement simple spi communication between 2 stm8s. Sending 0x04( address of pin2) and passing the received data as argument to GPIO high function so that LED connected at PORT D PIN 2 will glow. Master code is working properly, degugg...

Upate.1 by Associate II
  • 2608 Views
  • 4 replies
  • 0 kudos

Issue in reading the EEPROM data via SPI

Hi,We are using MPC5xxx uC and configured single SPI channel for 3 different devices. One of the device is EEPROM (M95256-DRE) and SPI channel is configured as 'Synchronous' mode.Issue : Before configuring the SPI channel for EEPROM, the two devices...

NC.1 by Associate
  • 728 Views
  • 1 replies
  • 0 kudos

Resolved! Exactly how much is endurance?

HiWe are using 95128-A125. It's datasheet provides "write cycle endurance" numbers for various operating temperatures. But there is a note that reads "The Write cycle endurance is defined for groups of four data bytes located at addresses [4*N, 4*N+1...

PRana.3 by Associate
  • 1355 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.