2010-03-09 6:36 AM
STM8S103F TIM1 CLK_PSC and CLK_CNT frequency not matching
2011-05-17 6:07 AM
2011-05-17 6:07 AM
I have figured out that this too is my problem, but using your suggestions, I can't get it fixed. I've tried adjusting the HSIDIV and the TIM1_ICPSC_DIV to no avail. Wouldn't making the ICPSC_DIV higher make it possible to capture faster signals, not slower? Or is my mind working backwards? I say this because the TIM will overflow more often with longer times between edges, i.e. slower freqs.
CLK_DeInit(); /* Configure the Fcpu to DIV1*/ CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1); /* Configure the HSI prescaler to the optimal value */ CLK_SYSCLKConfig(CLK_PRESCALER_HSIDIV1); /* Output Fcpu on CLK_CCO pin PE.0*/ CLK_CCOConfig(CLK_OUTPUT_HSI); CLK_CCOCmd(ENABLE); /* Initilize the Clock controller according to CLK_InitStructure 24MHz */ status = CLK_ClockSwitchConfig(CLK_SWITCHMODE_AUTO, CLK_SOURCE_HSE, DISABLE, DISABLE); while (CLK_GetFlagStatus(CLK_FLAG_HSERDY) == 0); TIM1_ICInit( TIM1_CHANNEL_1, TIM1_ICPOLARITY_RISING, TIM1_ICSELECTION_DIRECTTI, TIM1_ICPSC_DIV8, 0x0);We’re moving the ST Community to a new platform to give you a better and more reliable community experience.