2012-06-04 1:52 AM
I am using the UART1_Printf example from the STM8S Standard Peripheral Library version 2.1 and I am having problems with the speed of the UART. I am expecting to see 115200 baud but according to my logica analyser I am in fact seeing 53 baud (approx).
To double check the LA value I have fed the output from an independent system running .NETMF and asked it to produce a similar signal. The LA reports the right baud rate give or take a small deviation (i.e. 9615 baud).Is anyone else seeing similar problems or have a solution?Regards,Mark #uart-baud-rate2012-06-05 2:41 PM
I think I have found the problem, the BRR1 and BRR2 registers we not being set correctly. I hacked the stm8s_uart1.c library file and set the register values and it works.
regards,MarkWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.