2010-10-16 9:09 AM
STM8S PWM jitter
2011-05-17 6:11 AM
Hi klass,
Here below a code that I suggested in my previous message. This could help. I didn't compiled it but this is the idea. TIM1_DeInit(); /* Set TIM1 Frequency to 10 kHz (=2Mhz/200), thus 1 unit = 0.1ms */ TIM1_TimeBaseInit(200, TIM1_COUNTERMODE_UP, 2500, 0); /* TIM1 channel 1 is used (PC1) with rising edge and no divider nor filter */ TIM1_ICInit(TIM1_CHANNEL_1, TIM1_ICPOLARITY_RISING, TIM1_ICSELECTION_DIRECTTI, TIM1_ICPSC_DIV1, 0x0); /* the trigger input (TRGI) to used to synchronize the counter is TI1FP1: Filtered timer input 1 (TI1FP1) */ TIM1_SelectInputTrigger(TIM1_TS_TI1FP1); /* Reset mode - Rising edge of the selected trigger signal (TI1FP1 in this case) re-initializes the counter and generates an update of the registers. */ TIM1_SelectSlaveMode(TIM1_SLAVEMODE_RESET); /* Overflow interrupt after 250ms = 2500*0.1ms; Capture1 interrupt enabled */ TIM1_ITConfig(/*TIM1_IT_UPDATE | */TIM1_IT_CC1, ENABLE); /* generate an update event */ TIM1_GenerateEvent(TIM1_EVENTSOURCE_UPDATE); /* Clear CC1 and update Flag */ TIM1_ClearFlag(TIM1_FLAG_CC1 | TIM1_FLAG_UPDATE); /* Enable TIM1 */ TIM1_Cmd(ENABLE); /* enable global interrupts */ enableInterrupts(); /* Set the code below in TIM1 capture interrupt */ time = 10000/((double)TIM1_GetCapture1()); //by the way check that compiler is well handling this operation if (time > 180){ time = 180; } pwm = ((u16)50*time+1400); TIM2_SetCompare1(pwm); Herzlich, MCU Lufter2011-05-17 6:11 AM
hi lowpowermcu,
Your solution worked! Thanks a lot! I only added a filter to the input because my signal gets a bit noisy in the high rpm range. There was a caveat though. I'm using the STM8S discovery board and I hadn't noticed that TIMER1 Channel1 and 3 is occupied by the Touch sensing button. So I spent some hours checking and checking before I found that I could not put decent signals on those channels... and then I saw it... Haha If only I could buy you a beer now :) Klaas2011-05-17 6:11 AM
Hi klaas,
Felicitation !!! regards, MCU LüfterWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.