2018-06-27 9:18 AM
Hi,
I have an STM8L151F3 MCU on my board.
I'm trying to find info on the default USART pins for using the on-chip serial boot loader together with the flash loader demonstrator by ST.
There are 3 options and couldn't find any clue in any ST document.
Could someone help please.
Regards
2018-06-27 11:02 PM
Like UM0560 and the pin designations in the Data Sheets?
2 Boot ROM
This section applies to low-density STM8L05xx/STM8L15xx devices, medium-density STM8L05xx/STM8L15xx devices, medium+ density STM8L05xx/STM8L15xx devices and high-density STM8L05xx/STM8L15xx/STM8L16xx devices, unless otherwise specified.
The internal 2 Kbyte boot ROM contains the bootloader code. Its main task is to download the application program to the internal Flash/EEPROM through the USART1, USART2, USART3 (USARTs in asynchronous mode), SPI1 or SPI2 interfaces and program the code, data, option bytes and interrupt vectors in the internal Flash/EEPROM.
Refer to product datasheets for details on available communication ports.
To perform boot loading in LIN mode, a different bootloader communication protocol is
implemented on UART2/UART3 and UART1.
The boot loader starts executing after reset.
Refer to the STM8 bootloader user manual (UM0560) for more details.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.