2013-06-24 4:13 AM
Hello!
Have anybody any information on bootloader interface configuration for I couldn't find direct instructions on port connections. I assume they should be PC2 and PC3 pins (due to SYSCFG->RMPCR1 default value) but there is some problem: STM8LF151F3 in UFQFPN20 package have no these pins. So is it even possible to use bootloader in UART mode with this package or I should look towards usin SPI interface? By the way, which pins do bootloader require for SPI? Maybe PB5, PB6, PB7 ? #bootloader2014-05-06 2:10 AM
Hi,
did you find any answer to your question yet? We are stuck at the exact same point trying to use the STM8L151F3's bootloader.Best RegardsFlorianWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.