2011-10-08 10:29 PM
Hi all ,
I have try to compile default code ( discovery demo ) and everything runs fine. After which i try to create my own application following the guide : UM0991 <Building, debugging and running your application with STVD> page 47 onward. After the all the setting and work , i try to compile but was given the following error (i did not induce any code the main.c yet)... Any one knows what wrong ? Compiling ..\..\..\..\libraries\stm8l15x_stdperiph_driver\src\stm8l15x_gpio.c... rcstm8 ..\..\..\..\libraries\stm8l15x_stdperiph_driver\src\stm8l15x_gpio.c OBJECT(Debug\stm8l15x_gpio.o) PIN(''C:\Program Files\Raisonance\Ride\inc\STM8'') PIN(''C:\Program Files\Raisonance\Ride\inc\ST7'') PIN(''C:\Program Files\Raisonance\Ride\inc'') DGC(page0) AUTO WRV(0) PR(Debug\stm8l15x_gpio.lst) CD CO SB OT(0) DEBUG STM8(SMALL) PIN(..\..\inc) PIN(..\..\..\..\libraries\stm8l15x_stdperiph_driver\inc) RCSTM8 COMPILER V2.38.11.251 - Lite (32 Kb code limited) Copyright (c) Raisonance S.A.S. 1987-2011. All rights reserved. *** ERROR P028 IN LINE 54 OF ..\..\..\..\libraries\stm8l15x_stdperiph_driver\inc/stm8l15x.h : ''Please select first the target STM8L device used in your application (in stm8l15x.h file)'' RCSTM8 COMPILATION COMPLETE. 0 WARNING, 1 ERROR The command: ''rcstm8 ..\..\..\..\libraries\stm8l15x_stdperiph_driver\src\stm8l15x_gpio.c OBJECT(Debug\stm8l15x_gpio.o) PIN(''C:\Program Files\Raisonance\Ride\inc\STM8'') PIN(''C:\Program Files\Raisonance\Ride\inc\ST7'') PIN(''C:\Program Files\Raisonance\Ride\inc'') DGC(page0) AUTO WRV(0) PR(Debug\stm8l15x_gpio.lst) CD CO SB OT(0) DEBUG STM8(SMALL) PIN(..\..\inc) PIN(..\..\..\..\libraries\stm8l15x_stdperiph_driver\inc) '' has failed, the returned value is: 2 exit code=2. #um0991 #compilers2011-10-09 11:18 AM
''Please select first the target STM8L device''
So have you done that?''(in stm8l15x.h file)'' It even tells you where to do it!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.