2025-05-12 8:47 AM - last edited on 2025-05-14 1:50 AM by Andrew Neil
Hi, I use a PCB that is reduced to one STM8AF5288 and 3 100nF Capacitors. No other components, all are removed. I supply it with 3,3V. I want to reduce current consumption in halt-mode to 4,5uA. Some others posted simliar problems, I could never find a working solution. My current consumption in halt mode is:
350uA at 3V
550uA at 3,3
1050uA at 3,7
Here is my code, can anyone please help? I am really in trouble.
Thank you very much,
Holger
void main(void)
{
CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV8); // 2 MHz
GPIO_Init(GPIOA, GPIO_PIN_ALL, GPIO_MODE_IN_PU_NO_IT);
GPIO_Init(GPIOB, GPIO_PIN_ALL, GPIO_MODE_IN_PU_NO_IT);
GPIO_Init(GPIOC, GPIO_PIN_ALL, GPIO_MODE_IN_PU_NO_IT);
GPIO_Init(GPIOD, GPIO_PIN_ALL, GPIO_MODE_IN_PU_NO_IT);
ADC1->CR1=0x00;
CLK_PeripheralClockConfig(CLK_PERIPHERAL_ADC, DISABLE);
//Only Timer 1, 2 and 4 seem to exist
TIM1->CR1=0x00;
TIM2->CR1=0x00;
TIM4->CR1=0x00;
CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER1, DISABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER2, DISABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER4, DISABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_AWU, DISABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_UART1, DISABLE);
UART1->CR1 = 0x20;
UART1->CR3 = 0x00;
#define CAN_MCR (*((volatile uint8_t*)0x5420))
CAN_MCR = 0x02;
//CAN->MCR = 0x02; //This does not work, the above code is a workaround
CLK_PeripheralClockConfig(CLK_PERIPHERAL_CAN, DISABLE);
SPI->CR1=0x00;
CLK_PeripheralClockConfig(CLK_PERIPHERAL_SPI, DISABLE);
I2C->CR1 = 0x00;
CLK_PeripheralClockConfig(CLK_PERIPHERAL_I2C, DISABLE);
IWDG->KR =0x00;
WWDG->CR=0x00;
AWU->CSR = 0x00;
FLASH->CR1=0x00;
disableInterrupts();
CLK->CKDIVR = 0xFF; // max. Prescaler für CPU und Peripherie
__asm__("halt");
while (1)
{
}
}Post edited to apply source code formatting - please see How to insert source code for future reference.
Solved! Go to Solution.
2025-05-13 12:50 AM
I found the cause of high current. It is a wiring bug: I connected V_CAP to 3,3V. V_CAP must be 1,8V, there must only a capacitor be connected to V_CAP. So please close the topic.
2025-05-13 12:50 AM
I found the cause of high current. It is a wiring bug: I connected V_CAP to 3,3V. V_CAP must be 1,8V, there must only a capacitor be connected to V_CAP. So please close the topic.
2025-05-13 1:17 AM - edited 2025-05-13 1:18 AM
@HolgerG wrote:So please close the topic.
You do that by marking your post as the solution:
https://community.st.com/t5/community-guidelines/help-others-to-solve-their-issues/ta-p/575256
Please see also: How to insert source code.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.