2013-08-09 4:41 PM
Can anyone help me with the problem below dotted line? It seems like I need to set up memory spaces for the Micro Controller. Is that ? the problem. If so how do I fix? Thanks! GDN
------------------------------------------------------------- Running Linkerclnk -l''C:\Program Files\COSMIC\Lib'' -o Debug\i2c_iap.sm8 -mDebug\i2c_iap.map Debug\i2c_iap.lkf
#error clnk Debug\i2c_iap.lkf:1 no default placement for segment .MAIN_CODE
#error clnk Debug\i2c_iap.lkf:1 no default placement for segment .SPI_CODE
#error clnk Debug\i2c_iap.lkf:1 no default placement for segment .CLK_CONST
#error clnk Debug\i2c_iap.lkf:1 no default placement for segment .CLK_CODE
#error clnk Debug\i2c_iap.lkf:1 no default placement for segment .I2C_CODE
#error clnk Debug\i2c_iap.lkf:1 no default placement for segment .I2C_CONST
#error clnk Debug\i2c_iap.lkf:1 no default placement for segment .GPIO_CODE
#error clnk Debug\i2c_iap.lkf:1 no default placement for segment .FLASH_CODE
The command: ''clnk -l''C:\Program Files\COSMIC\Lib'' -o Debug\i2c_iap.sm8 -mDebug\i2c_iap.map Debug\i2c_iap.lkf '' has failed, the returned value is: 1
exit code=1.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.