2026-03-13 9:58 PM - last edited on 2026-03-14 2:41 AM by Andrew Neil
Hi Guys,
Based on some tutorials, I am trying to execute ADC module of STM8S105 and display the ADC result in 16x2 LCD display. The problem is : thousandth digit place is showing alphabetic character right from "A" when I increase voltage on ADC channel from 0. Please see my code as well as adc.h file. I am eagerly awaiting someone to suggest where I have made the mistake.
#define LCD_RS GPIOD, GPIO_PIN_2
#define LCD_EN GPIOD, GPIO_PIN_3
#define LCD_DB4 GPIOD, GPIO_PIN_4
#define LCD_DB5 GPIOD, GPIO_PIN_5
#define LCD_DB6 GPIOD, GPIO_PIN_6
#define LCD_DB7 GPIOD, GPIO_PIN_7
#include "STM8S.h"
#include "lcd.h"
#include "adc1.h"
main()
{
//Variable declarations
unsigned int test_var ;
char d4,d3,d2,d1;
gpio_adc_init();
adc_init();
Lcd_Begin();
Lcd_Clear();
Lcd_Set_Cursor(1,1);
Lcd_Print_String("STM8S103F3P3 LCD");
delay_ms(5000);
Lcd_Clear();
Lcd_Set_Cursor(1,1);
Lcd_Print_String("Circuit Digest");
Lcd_Set_Cursor(2,1);
Lcd_Print_String("Test: ");
while (1)
{
test_var = read_adc_value();
d4 = test_var%10 + '0';
d3 = (test_var/10)%10 + '0';
d2 = (test_var/100)%10 + '0';
d1 = (test_var/1000) + '0';
Lcd_Set_Cursor(2,6);
Lcd_Print_Char(d1);
Lcd_Print_Char(d2);
Lcd_Print_Char(d3);
Lcd_Print_Char(d4);
delay_ms(1000);
//test_var++;
}
}
#ifdef USE_FULL_ASSERT
void assert_failed(uint8_t* file, uint32_t line)
{
while (1)
{
}
}
#endifadc.h
uint16_t value;
void gpio_adc_init(void) {
CLK_PeripheralClockConfig(CLK_PERIPHERAL_ADC, ENABLE);
GPIO_Init(GPIOB, GPIO_PIN_4, GPIO_MODE_IN_FL_NO_IT);
}
void adc_init(void) {
ADC1 -> CSR = 0x04;
ADC1 -> CR1 = 0x40;
ADC1 -> CR2 = 0x00;
ADC1 -> TDRH = 0xFF;
ADC1 -> TDRL = 0xFF;
ADC1 -> CR1 |= ADC1_CR1_ADON;
}
uint16_t read_adc_value(void) {
// Start the conversion process
ADC1_StartConversion();
// Wait until the end of conversion (EOC) flag is set
while(ADC1_GetFlagStatus(ADC1_FLAG_EOC) == FALSE);
// Read the 10-bit value (clears the EOC flag automatically when the data registers are accessed correctly)
value = ADC1_GetConversionValue();
ADC1_ClearFlag(ADC1_FLAG_EOC); // Explicitly clear the flag if needed, depending on read method and mode
return value;
}
Solved! Go to Solution.
2026-03-16 7:37 AM
The column advances because the HD44780‑compatible LCD controller automatically moves the cursor after each character write, not because Lcd_Set_Cursor() is called multiple times. Therefore, d1, d2, d3 and d4 appear in consecutive columns (6, 7, 8, 9) even though the cursor is explicitly set only once in the code.
The ADC function is unrelated; it merely provides the data that you later display.
2026-03-17 6:27 AM
Thanks Peter.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.