2019-07-23 2:59 AM
Hi,
I am testing an application, and currently is working properly with HSI configured to 16MHz.
Now I want to enable the HSE.
I am using a NUCLEO-8S208RB. I have soldered an external crystal on X2, and i have configured the board with 12pF capacitors and 0 ohms resistor.
The crystal has a resonance frequency of 24 MHz. Configuring the firmware in order to output the clock frequency from pin 57 of STM8S (CLK_CCO), everything seems working (i can see the 24MHz synusoid with the oscilloscope).
Unfortunately the microcontroller is not working, because the application doesn't run.
I have configured the HSE clock in this way:
CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1);
CLK_SYSCLKConfig(CLK_PRESCALER_HSIDIV1);
/* Output Fcpu on CLK_CCO pin */
CLK_CCOConfig(CLK_OUTPUT_CPU);
/*Enable external oscillator*/
CLK_ClockSwitchConfig(CLK_SWITCHMODE_AUTO, CLK_SOURCE_HSE, DISABLE, CLK_CURRENTCLOCKSTATE_DISABLE);
CLK_HSECmd(ENABLE); //I have some doubts about this...is it really needed?
Do you see anything wrong?
Best regards
Solved! Go to Solution.
2019-07-23 11:53 PM
I have managed to solve this problem: in the datasheet (DocID14733 Rev 13 page 49), in the Option bytes section it is written that in order to use an HSE with a frequency higher than 16MHz you need to put the option byte WAITSTATE to 1 (OPT7).
2019-07-23 11:53 PM
I have managed to solve this problem: in the datasheet (DocID14733 Rev 13 page 49), in the Option bytes section it is written that in order to use an HSE with a frequency higher than 16MHz you need to put the option byte WAITSTATE to 1 (OPT7).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.