2005-01-13 1:27 AM
2004-12-08 9:09 PM
Hi,
Is anybody able to explain what does the statup routine provided by the Metrowerks Codewarrior C compiler ? I'm using it with the inDART-STX and, in debbug mode,when I ''run'' the code directly at statup, it bugs and say ''communication problem'' when I stop it. On the other hand, when I change the source file and make ''run to cursor'' in the ''main'' routine or if I run it through ''Steps'', it works properly ! :o Does anybody already had this problem ? Is it comming from the startup routine or am I making mistakes in the memory configuration ? Thanks for your help.2005-01-13 1:27 AM
Depending of th type of Flash on your ST7 (XFlash and HDFlash) and if the ST7 is equiped with the Debug Module the limitations of the ICD are different.
Last running or stepping with InDart are in fact two different way of operating. The best is to contact Softec support (support@softecmicro.com) which will be pleased to help resolve your issue. Best regards, AlainWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.