2005-01-12 11:52 PM
2005-01-11 11:48 PM
Hi All
I am having trouble getting the CAN module to work. By using the following code to initialise the module in loop back mode I can see transmitted messages correctly using a can bus monitor. Also a receive interrupt gets generated each time I transmit a message. void Can_Init(void) { GPIO_Config(GPIO1,(1< GPIO_Config(GPIO1,(1< CAN->CR = CAN_CR_CCE | CAN_CR_INIT | CAN_CR_TEST; CAN->TESTR=0x0010; // set loopback mode to test CAN->SR = 0; // reset the status CAN->BRPR = 0; CAN->BTR=0x34d7; // 100kbits @ 24Mhz clk CAN_InvalidateAllMsgObj(); SetMessageObjects(); // set message object 1 to transmit and 2- 32 as receive fifo CAN->CR = CAN_CR_IE | CAN_CR_TEST ; } Because it works fine in loop back mode I assume I have the message objects setup correctly. Now when I set CAN->TESTR=0x0000; and CAN->CR = CAN_CR_IE; at the end of Can_Init(). After I do this I no longer see CAN messages externally. I dont get a receive interrupt if I send CAN messages to the board. I dont get a ''message transmitted ok'' in the CAN_SR register The CAN_TRnR register has the correct bit set to indicate I have requested a transmit. The CAN_NDnR register has the corresponding bit cleared, even though I set it in the transmit. Is it cleared by the CAN module ? The CAN_MVnR register has the correct bit to indicate the message object is valid. I am confused as to why I can get CAN messages in test mode with loop back enabled but as soon as I come out of test mode nothing appears to work. Also if I stay in test mode but dont enable loop back (CAN_TESTR = 0) I still get no CAN externally even though from the data sheet I would expect some as bits 5 & 6 indicate the CAN_TRX pin is controlled by the CAN moudle. I have spent a day trying to get this to work and as far as I can see I am not doing anything wrong. thanks for any help Ben,2005-01-12 11:52 PM
Ok have now got it working.
Think the data sheet could be a little clearer. I was setting GPO1.11 (CAN RX) to alternate function when it needs to be an input. Had there been no alternate function option I would have set GPO1.11 to an input and wouldnt have had this trouble. Have left GPO1.12 (CAN TX) configured as alternate function.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.