2005-03-15 8:41 PM
ST92F150 with external SRAM 32K: problems
2011-05-17 2:36 AM
Hi professionals,
we're using the ST92F150CV1 for about 18months in production (about 1000 pieces). Suddenly we have problems with the external SRAM: it's no more possible to write data in it. Facts:CPU-Speed: 12MHz, Core-Speed: 6MHz, DS-strecht: MAX, AS-Strech: MAX mode control: Mode=0, ETO=off, BSZ=1, circuit as in ST9-Datasheet V4, page 143, mode=0 ram: div. manufacturers (samsung, issy), 70ns and 55ns the messured cycle-time is about 1usec (very slow!) playing with waitstates, different configurations, different rams shows no way to fix the problems. on some boards reducing waitstates (as/ds) brings success, but not on the others. mode=1 (with rewiring AS to ALE) brings success on one board, but not on the others. are there any known (but inofficial) timing-probs with the EMI?(such as the new chapter ''KNOWN LIMITATIONS'' in datasheet V4? (app notes an1069 + an1076 are well known). has anybody successfull created a board with such a configuration?need help!2011-05-17 2:36 AM
Hi,
it seems to be a timing-problem with R/W. in mode=1 (and removing the inverter for AS->ALE) the sram runs perfectly. unfortunately, we can't switch the design to mode=1, cause on the same data/adressbus there's a graphic-LCD which doesn't run with mode=1. And: sram should work with mode=0 (as shown in datasheets)! :-W anybody any hints?2011-05-17 2:36 AM
hi there,
another facts (problem is still existing): i attached diagramms of 4 accesses to the sram: 2x write: - write AD=2, Data=1 - write AD=3, Data=2 2x read - read AD=2: >> Data=3 (fail!!!)- read AD=3: >> Data=2 (correct) why doesnt work the first write? the naming conventions are for sram, the mode in st9 is mc=0 (oe/ which is ds/ from st9 has one cycle in mc=0). and, as you can see in the diagramms, all waitstates are activated, so access is slow. what is wrong in first write-access?thank you professionals! siggiWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.