2003-12-04 9:05 PM
2003-12-02 2:41 AM
I am running an ST72F324 with an external 16MHz crystal and need this speed for performing complex alogrithms.
The problem is that during EMC testing there are peaks at harmonics of 16MHz which are over the limit, that I'm sure are coming from the ST7. I am using a 2 layer board with ground plane and close decoupling. Would I benifit using the PLLx2 and a 4MHz crystal to reduce these peaks or are there other things I can do2003-12-04 3:52 AM
Could you give me the exact name of the device?
thanks.2003-12-04 9:05 PM
The part no of the device is
ST72F324K2T6We’re moving the ST Community to a new platform to give you a better and more reliable community experience.