2004-02-10 7:55 PM
2004-02-10 4:48 PM
dear sir,
I have some doubt regarding ''ST72264G'' datasheet.I have found some ambiguity in the ''Memory Map''(page 10) section.In that doc Memory map is divided into 5 parts- * HW Registers(0000h-007fh) * RAM(0080-017fh) * Reserved(0180h-Dfffh) * Program Memory(E000h-Ffdfh) * Interrupt & Reset Vectors(FFE0h-FFFFh) In the same page u have showed program memory is divided into 2 parts: sector 1(E000h-EFFFh) sector 0(F000h-FFFFh) which is reserved for interrupt & reset vectors. while Program Memory space itself is E000h-FFDFh,then how can be one of its part sector 0 which is in the space F000h-FFFFh is lying outside the program memory space. While already you have showed Progarm Memory and Reset & Interrupt vector space as two distinct part in the memory map,then why did u combine it with sector 0 of progarm memory. Pls exaplain.And rectify it in your ST72264G Doc. Regards, Arup2004-02-10 7:55 PM
It does not impact the application anyway and it is same terminology which is used in all ST7 devices.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.