2004-05-04 9:43 PM
2004-03-21 11:43 PM
In the Simulator Memory window is the possibility to save the memory to a file, and reload this file.
I would like to use this feature during debugging where I have to put in start values in diff. places in RAM0 page. If I reload the file I have saved before I cant start the simulation (Error: the program is not being run). Can anyone help me? regard Kurt2004-03-28 10:40 PM
We do seem to be having a problem. However, it is solved if after the ''File>Restore layout'' option you do a chip-reset and then execute application.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.