2004-11-26 7:51 PM
2004-11-10 9:11 PM
Hi to all,
I have seen on ST brochure an abbreviation ''SCI'' on ST72264G micro. Can I use it like a UART comunication with PC (through MAX232) ? Tanks in advantage!! MBKS2004-11-10 11:05 PM
Hi MBKS,
I use SCI on the ST72334 and it's easily done with 8bits (7bits+parity). Didn't examine with 8bits+parity but I think it runs as well, certainly a little bit more complicated. The SCI has at least the same features as a good UART. If you use the MAX232 you should have no restrictions on communicating on any asynchronous serial communications interface you want, even full-duplex. Regards WoRo2004-11-26 7:51 PM
Hi,
I'm using SCI in the 8+1 bit 38900 baud mode, full-duplex. Works very fine. I've also used it at 9600 bauds without problem. As already said you just need a MAX232 or similar part, and the transmission is done without RS232 control signals, only Tx and Rx. There is an AN about the SCI usage. [ This message was edited by: alpa on 27-11-2004 09:34 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.