2004-02-05 11:23 PM
ST62T65 problem with ports and interrupts
2004-02-05 5:16 AM
I work with 4 interrupts simltaneously: NMI
AR Timer A/D Converter TIMER My ports have next configuration: DDRA 11110000 DDRB 11111111 DDRC 00000010 ORA 11110010 ORB 00111111 ORC 00000010 DRA 11110110 DRB 11111111 DRC 00000011 All interrupt works in real time. My problem is: When I reconfigure outputs of port B in Timer (or A/D converter) interrupt, then interrupt of AR timer is not periodical. All the time I have in ARCP register the same value. My AR Timer works in auto-reload mode, and makes compare interrupt. What I must do, to interrupt of AR Timer was periodical, and independent from reconfiguration port B in vector 4 interrupt.2004-02-05 11:23 PM
When you configure the timer intrerrupt, this makes the timer interrupt to occur after the particular time. Also at the same time you are also enabling ARtimer interrupt.
The ARtimer interrupt in this case in not periodical. This is due to the fact that if the ARtimer interrupt occur when the controller is executing Timer Interrupt service routine, then first the timer interrupt routine will get executed and after completing the Timer ISR, the control will go to ARTimer routine or any other ISR depending on the priority of the interrupt.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.