2006-02-22 12:47 AM
st10f269 code Temporary Unprotection
2006-02-21 11:59 PM
hi,
Once Code Protection Set in St10F269,then what is the exact sequence to reprogram it using St10 Flasher and Code Temporary Unprotection command?2006-02-22 12:47 AM
Hello,
Once Code Protection is set in the ST10F269, it is no longer possible to use the ST10Flasher tool ,as it is, to reprogram the flash. In order to be able to use the ST10Flasher tool to reprogram the flash after being protected, we should update the monitor source ... and the Code Temporary Unprotection command must be located in an unused location (that will never be erased) in the flash to be called when needed. Regards, Najoua. [ This message was edited by: Najoua on 22-02-2006 15:27 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.