2005-06-16 3:52 AM
2005-04-04 10:11 AM
hello.
i have another problem: after activating protection setting the uprog bit i can not write to internal flash anymore. my writing function is located in external RAM and works without protection. To temporary unprotect i write a #0 to adress 0 like MOVB RL4,#00h MOV R5,#00h MOV R10,#00h EXTS R10,#01h MOVB [R5],RL4 but after this my steak command returns with ''protection active'' error... (the code above shure is executed in internal flash!) Which adresses do i have to set to zero to unprotect the flash temporary? kindest regards, itsme [ This message was edited by: itsme on 04-04-2005 22:43 ]2005-04-04 11:05 PM
1.
is it necessary to deprotect ST10F168 temporary to use the SFR ZEROS or is it enough to write a zero VALUE to an even address? 2. Is a MOVB also ok or DO i need a WORD-Instruction MOV ? 3. Is it possible to use indirect adressing or DO i need DIRECT ADRESSING? I protect two mcu until now with missing right deprotection in internal flash. is there a way to deprotect (temporary) in another way or erase whole internal flash and protection bit or can i throw them to the ''waste-can''?! [ Diese Nachricht wurde editiert von : itsme on 05-04-2005 12:34 ]2005-06-16 3:52 AM
No, it seems that it MUST be the ZEROS register!
Anyway, nevertheless i have problems with unprotection. If i run a program in internfal flash like: exts #3,#1 mov 08000h,ZEROS [...] copy some flash functions to memory [...] calls _erasepage (located in memory) this works fine and the page is erased. if i locate following procedure in internal flash and call it from external memory it does not work... curious... example iflash: org 038000H exts #3,#1 mov 08000h,ZEROS rets external memory: calls seg _038000, sof 38000h ; unprotect ..erasepage... errorcode: flash protected... ?! How is this possible... There are things between zero and one i do not understand... ;)We’re moving the ST Community to a new platform to give you a better and more reliable community experience.