2008-02-20 1:51 PM
ST10276Z5Q3 Interrupt service problem
2008-02-19 7:17 PM
Hello!
In my ST10F276 application,the CAPCOM12 interrupt routine defined as following: void KeyPressed (void) interrupt CC12INT=0x1C { //do some thing ... } In system initial routine ,the following code are added: sbit CCMOD12_0 = CCM3^0; sbit CCMOD12_1 = CCM3^1; sbit CCMOD12_2 = CCM3^2; CC12IC = 0x1E; //0111 10 ILVL=7, GLVL=2 _nop_();_nop_();_nop_(); CCMOD12_0 = 0; _nop_();_nop_();_nop_(); CCMOD12_1 = 1; _nop_();_nop_();_nop_(); CCMOD12_2 = 0; _nop_();_nop_();_nop_(); CC12IE = 1; _nop_();_nop_();_nop_(); IEN = 1; _nop_();_nop_();_nop_(); But the interrupt service routine never execute when I change CC12IO level from 0V to 5V or from 5V to 0V. Can anyone help? thanks!2008-02-20 1:51 PM
Add the folowing code:
CC12IR = 1;We’re moving the ST Community to a new platform to give you a better and more reliable community experience.