2002-12-03 1:25 AM
2002-12-02 7:16 PM
Dear All,
I am new of ST MCU. Now I use the ST7 visual debug simulator to implement a PWM funciton on ST7Lite But I found there was some problem. I can not look at the wave form in ST7 wave form editor. could anyone help me? the part source code are as bellows: main call init ; port initialization call init_pwm .loop jra loop .init ld A, $1F ld PADDR, A ; configures port A[0..4] as output ld PAOR, A ld A, $07 ld PBDDR, A ; configures port B[0..2] as output ld PBOR, A ld A, $23 ; enables the A/D peripheral on PB3 ld ADCCSR, A ret .init_pwm ld A,0 ; 0 0 0 0 0 0 OP0 CMPF0 ld PWM0CSR,A ; bit 1 set the PWM invert or noinvert ld A,8 ld ATRH ld A,0 ld ATRL,A ;set ART, ie. set the PWM frequency ld A,15 ld A,DCR0H ld A,1 ld DCR0L,A ;Set PWM duty cycle ld A,$10 ld ATCSR,A ; ld A,1 ld PWMCR,A ;bit 0=1 PWM output enabled. ret segment 'vectit' DC.W 0 ; FFE0-FFE1h DC.W 0 ; FFE2-FFE3h DC.W 0 ; FFE4-FFE5h DC.W 0 ; FFE6-FFE7h DC.W 0 ; FFE8-FFE9h DC.W 0 ; FFEA-FFEBh DC.W 0 ; FFEC-FFEDh DC.W 0 ; FFEE-FFEFh DC.W 0 ; FFF0-FFF1h DC.W 0 ; FFF2-FFF3h DC.W 0 ; FFF4-FFF5h DC.W 0 ; FFF6-FFF7h DC.W 0 ; FFF8-FFF9h DC.W 0 ; FFFA-FFFBh DC.W 0 ; FFFC-FFFDh DC.W main2002-12-03 1:25 AM
Hi,
The simple answer is that the PWM is not running. A small change is required: .init_pwm ld A,DCR0H should be ld DCR0H, A regards, Simon Anglia Internal Apps SupportWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.