2007-02-27 9:13 AM
SSPx frequency calculation error
2011-05-17 12:36 AM
Hi,
I think there may be a slight error in rev1 of the reference manual. In section 10.4.6 (page 238), the following is quoted:Quote:
The serial bit rate is derived by dividing down the input clock PCLK. The clock is first divided by an even prescale value CPSDVSR from 2 to 254, which is programmed in SSP_PR. The clock is further divided by a value from 1 to 256, which is 1 + SCR, where SCR is the value programmed in SSP_CR0. The frequency of the output signal bit clock SCLK is defined below: fSCLK=fPCLK / (CPSDVR + (1+SCR)) For example, if PCLK is 3.6864MHz, and CPSDVSR = 2, then SCLK has a frequency range from 7.2kHz to 1.8432MHz. However, I think the formula should read fSCLK=fPCLK / (CPSDVR x (1+SCR)) to obtain the frequency range specified? Martin.2011-05-17 12:36 AM
While on this general area I reported a bug while back which is pretty fundamental in the HAL. Never sure if my bug reports make it to the relevant people, so...
code snipit from 91x_ssp.c... /* Configure the Mode */ if(SSP_InitStruct->SSP_Mode == SSP_Mode_Slave) { /* Set the slave mode */ SSPx->CR1 |= SSP_Mode_Slave; /* Configure the Slave output */ if(SSP_InitStruct->SSP_SlaveOutput == SSP_SlaveOutput_Disable) { /* Slave output disabled */ SSPx->CR1 |= SSP_SlaveOutput_Disable; } else { /* Slave output enabled */ SSPx->CR1 &= SSP_SlaveOutput_Enable; } } else { /* Set the master mode */ SSPx->CR1 &= SSP_Mode_Master; /* Clear clock rate SCR[7:0] bits */ SSPx->CR0 &= SSP_ClockRate_Mask; /* Set the serial clock rate */ SSPx->CR0 |= (SSP_InitStruct->SSP_ClockRate< /* Clear clock prescaler CPSDVSR[7:0] bits */ SSPx->PR &= SSP_ClockPrescaler_Mask; // WRONG, applicable to slave mode as well /* Set the serial clock prescaler */ SSPx->PR |= SSP_InitStruct->SSP_ClockPrescaler; // WRONG, applicable to slave mode as well } SSPx->PR only gets set up in master mode, but not in slave. The consequences on Rev D silicon are pretty harsh. random reboots, ARM core total lockups, total loss of JTAG comms, it's major league stuff. Also as a side note, running at a PCLK of 96MHz just doesn't fly with the SSP peripheral, it's unstable. 48MHz is far more friendly.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.