2005-11-15 10:28 PM
2005-11-15 10:10 PM
Hello
I have SPI master board, connected to the PC and send bytes to my application which run on ST7. I sent one byte at the time from the PC, and poll to get it on the ST7. I see that I have ''shift in the data''. for example, When PC send 0x32 = 0b00110010, ST7 gets 0x64 = 0b01100100, or when PC send 0x33 = 0b00110011, ST7 gets 0x66 = 0b 01100110. (I use CPOL=0 CPHA=1 and the speed is very low 5Khz to 62Khz) The ST7 configurate as slave in software SSM=1 SSI=0, and the /SS pin is used as floating input GPIO (but currently not used) Any hint ? Yours Oren2005-11-15 10:28 PM
Hello
forgot to mention, it can be shit by one in other direction, e.g. 0x32 = 0b00110010 becomes 0x19 = 0b00011001 :-[ OrenWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.