cancel
Showing results for 
Search instead for 
Did you mean: 

SPI question

henrik239955
Associate II
Posted on March 29, 2006 at 06:18

SPI question

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
henrik239955
Associate II
Posted on March 28, 2006 at 06:08

In my application I use SPI interface to transfer data between a ST7234 and a STLITE09. ST7234 is master and LITE09 acts as slave. What happens if a false clock pulse occurs on the SCK line (in a noisy environment for example)? The communication will be out of sync until new reset? Is there any way to recover from this without re-start the slave?

BR

bood

info45
Associate II
Posted on March 28, 2006 at 19:09

Hy,

You don't have problems with spike on clock, IF and only IF the Chip select on SPI slave is inactive (high state).

Bye

henrik239955
Associate II
Posted on March 29, 2006 at 05:48

Thanks for reply. I dont get your point. No matter how you manage chip select I think there is a risk of spikes when the chip is selected?

Chip select (SS) on my slave is managed by software and allways active (0).

bood

info45
Associate II
Posted on March 29, 2006 at 06:13

Hy Bood,

I prefer manage slave SS active only during spi communication.

So I have a hw/sw robustness: spike on signals are allowed without desyncronization.

If in Your application need to keep slave SS low, then Your hw/sw is spike sensible....

Bye

henrik239955
Associate II
Posted on March 29, 2006 at 06:18

OK, thank you.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.