2005-11-13 3:08 PM
SPI interface at 10MHz speed: delay between bytes transmitting
2011-05-17 3:09 AM
Hi,
I am trying to interface uPSD3334D Controller and SPI ADC Chip(TLC3578 from TI). I am able to communicate with ADC at less than 2.5MHz speed. When I increase the speed, from first byte and second byte a delay of more than 30uSec is coming. I am using the code I received with ST development kit as reference. Please help. I am attaching the modified code. Thanks. Jose void SPI_Init(void) { P4SFS0 = 0xF0; P4SFS1 = 0xF0; SPICON1=0x00; SPICLKD=0x04; SPICON0=0x18; IEA|=0x40; IPA|=0x40; EA=1; } void spiRead() { SPI_transfer(&INITIALIZE,0,2); //0xA0,0X00 SPI_transfer(&CONFIGURE,0,2); //0XAE, 0X42 SPI_transfer(&READ_FIFO,&RDFF_RX,16); //0XE0,0X00 } void SPI_transfer(unsigned char *send, unsigned char *receive, unsigned char length) { tlength = length; buf1 = send; buf2 = receive; flag1 = *buf1; flag = 0; endflag = 0; while (SPISTAT & SPI_BUSY_FLAG); SPITDR = *buf1; buf1++; tlen = 1; rlen = 0; SPICON1 |= RIE; SPICON1 |= RORIE; SPICON1 |= TEIE; SPICON1 |= TIE; SPICON0 |= TE; SPICON0 |= RE; } void SPI_isr (void) interrupt SPI_VECTOR using 2 { unsigned char status ; status = SPISTAT; if(status & SPI_TRANSMIT_END_FLAG) { while (SPISTAT & SPI_BUSY_FLAG); SPICON1 &= (~TIE); SPICON0 &= (~TE); SPICON1 &= (~TEIE); endflag = 1; } if(status & SPI_TI_FLAG) { if(tlen < tlength) { SPITDR = *buf1; buf1++; tlen++; } } if(status & SPI_RI_FLAG) { *buf2=SPIRDR; buf2++; rlen++; } } return 0; }2011-05-17 3:09 AM
In the code I am waiting at only following locations
while (SPISTAT & SPI_BUSY_FLAG); //to start transmission while (SPISTAT & SPI_BUSY_FLAG); //transmit complete I think I am not waiting anywhere else Thanks. JoseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.