2024-12-13 5:21 AM - last edited on 2024-12-13 5:36 AM by mƎALLEm
First of all, thank you all in advance, I am trying to control IKCM15L60GA IPM with Stm32f429.
I have added the circuit diagram below, my problem is that when I start the 250 W asynchronous motor drive process that I connected to the IPM output, it vibrates and remains fixed as if it is braked, it does not turn.
I will add the logic analyzer samples and other details as a file.
PLEASE HELP.
2024-12-13 5:22 AM - last edited on 2024-12-13 5:36 AM by mƎALLEm
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2024 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include <math.h>
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define TIMER_PERIOD 35999 // 5 kHz PWM için
#define SQRT3 1.73205080757
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
TIM_HandleTypeDef htim1;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_TIM1_Init(void);
/* USER CODE BEGIN PFP */
void SVM_Update(float Vd, float Vq);
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
void SVM_Update(float Vd, float Vq)
{
float T1, T2, T0;
float Va, Vb, Vc;
float sector;
// Üç faz referans gerilimlerini hesapla
Va = Vd;
Vb = -0.5 * Vd + SQRT3 / 2 * Vq;
Vc = -0.5 * Vd - SQRT3 / 2 * Vq;
// Sektör belirleme
if (Va >= 0 && Vb >= 0)
sector = 1;
else if (Vb >= 0 && Vc >= 0)
sector = 2;
else if (Vc >= 0 && Va >= 0)
sector = 3;
else if (Va < 0 && Vb < 0)
sector = 4;
else if (Vb < 0 && Vc < 0)
sector = 5;
else
sector = 6;
// Aktif ve sıfır vektör sürelerini hesapla
T1 = TIMER_PERIOD * fabs(sin(sector * M_PI / 3));
T2 = TIMER_PERIOD * fabs(sin((1.0 / 3.0 - sector) * M_PI));
T0 = TIMER_PERIOD - (T1 + T2);
// CCR değerlerini hesapla
uint32_t CCR1 = (uint32_t)((T0 / 2.0 + T1) / TIMER_PERIOD * TIMER_PERIOD);
uint32_t CCR2 = (uint32_t)((T0 / 2.0 + T2) / TIMER_PERIOD * TIMER_PERIOD);
uint32_t CCR3 = (uint32_t)((T0 / 2.0) / TIMER_PERIOD * TIMER_PERIOD);
// Timer 1 PWM kanallarını güncelle
__HAL_TIM_SET_COMPARE(&htim1, TIM_CHANNEL_1, CCR1);
__HAL_TIM_SET_COMPARE(&htim1, TIM_CHANNEL_2, CCR2);
__HAL_TIM_SET_COMPARE(&htim1, TIM_CHANNEL_3, CCR3);
}
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
if (htim->Instance == TIM1)
{
static float angle = 0.0;
float Vd = 0.8 * cos(angle);
float Vq = 0.8 * sin(angle);
angle += (2 * M_PI * 40 / 5000); // 50 Hz motor frekansı, 5 kHz taşıyıcı frekansı
if (angle > 2 * M_PI)
angle -= 2 * M_PI;
SVM_Update(Vd, Vq);
}
}
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_TIM1_Init();
// PWM çıkışlarını başlat
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_2);
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_3);
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_1);
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_2);
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_3);
// Timer interrupt başlat
HAL_TIM_Base_Start_IT(&htim1);
while (1)
{
// Ana döngü kullanılmıyor, tüm işlemler kesmelerle yapılır
}
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 4;
RCC_OscInitStruct.PLL.PLLN = 180;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 4;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
Error_Handler();
if (HAL_PWREx_EnableOverDrive() != HAL_OK)
Error_Handler();
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK|
RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
Error_Handler();
}
/**
* @brief TIM1 Initialization Function
* @retval None
*/
static void MX_TIM1_Init(void)
{
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};
htim1.Instance = TIM1;
htim1.Init.Prescaler = 0;
htim1.Init.CounterMode = TIM_COUNTERMODE_CENTERALIGNED1;
htim1.Init.Period = TIMER_PERIOD;
htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim1.Init.RepetitionCounter = 0;
HAL_TIM_Base_Init(&htim1);
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig);
HAL_TIM_PWM_Init(&htim1);
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig);
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 0;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1);
HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_2);
HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_3);
sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
sBreakDeadTimeConfig.DeadTime = 5;
sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig);
HAL_TIM_MspPostInit(&htim1);
}
/**
* @brief GPIO Initialization Function
* @PAram None
* @retval None
*/
static void MX_GPIO_Init(void)
{
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOE_CLK_ENABLE();
}
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
__disable_irq();
while (1)
{
}
}
2024-12-13 5:38 AM - edited 2024-12-13 5:38 AM
Hello @Sözde.11 ,
In next time please use </> button to paste your code: https://community.st.com/t5/community-guidelines/how-to-insert-source-code/ta-p/693413
I've edited your post to be inline with the community rules.
Thank you.
2024-12-13 5:39 AM
Hi, I didn't know it was like this, thank you for your help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.