cancel
Showing results for 
Search instead for 
Did you mean: 

SG3525AN spice circuit

SMusc.1
Senior

Hi, there is a way to found the spice model for the IC: SG3525AN?

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

I'm afraid I have to tell you that there isn't a Spice model for such an old-timer from the last millennium.

It’s a shame I can’t give you a more positive answer.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

I'm afraid I have to tell you that there isn't a Spice model for such an old-timer from the last millennium.

It’s a shame I can’t give you a more positive answer.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks anyway but I managed to find the template on the web and I'm attaching it in case anyone needs it

* PSpice Model Editor - Version 16.6.0

*$
*  
.subckt sg3525a INV NI SYN OSC CT RT DCH SS CMP SHD OUA GND VC OUB VIN VRF
A1 N017 0 N009 0 0 N017 N020 0 DFLOP Vhigh=5.1 Trise=20n Rout=30
A2 N018 N019 N009 0 N020 N005 N011 0 OR Vhigh=5.1 Trise=400n Rout=30
A3 N017 N009 0 N019 N018 N023 N022 0 OR Vhigh=5.1 Trise=400n Rout=30
S1 OUA N004 N005 0 HOUT
S2 N012 OUA N011 0 LOUT
S3 OUB N021 N023 0 HOUT
S4 N028 OUB N022 0 LOUT
I1 N031 0 21m
D1 0 N031 IDEAL
R1 N029 N031 8.93
R2 N029 0 22.6
D2 N029 N032 D1_75
D3 0 N032 IDEAL
I2 N032 0 188m
R3 N032 0 2.28
D4 N028 N029 IDEAL
I3 N014 0 21m
D5 0 N014 IDEAL
R4 N013 N014 8.93
R5 N013 0 22.6
D6 N013 N015 D1_75
D7 0 N015 IDEAL
I4 N015 0 188m
R6 N015 0 2.28
D8 N012 N013 IDEAL
D9 VC N021 IDEAL
D10 VC N004 IDEAL
G1 0 N024 NI N027 table=(-70m -100u,0 0,70m 100u)
R7 N024 0 4meg
C1 N024 0 100p
R8 N024 CMP 30
R9 INV 0 1meg
R10 NI 0 1meg
I7 0 VRF 80m
R11 VRF 0 170
D11 0 VRF Z5_1
D12 0 VC Z40
A4 VIN 0 0 0 0 N001 0 0 SCHMITT Vhigh=5.1 Vlow=0.45 Trise=20n Vt=7.25 Vh=0.25
I8 VIN 0 TBL(0 0 3 3.8m 7 19m 8 20m 40 24.1m)
D13 N030 N024 Z5_6
V1 N030 0 0.2
R12 N036 0 5k
R13 SHD N002 5k
Q1 SS N002 N036 0 NPN
D14 N002 0 D1_2
R14 N001 N002 60k
D15 0 SS Z5_1
I9 0 SS 50µ
A5 N002 0 0 0 0 0 N019 0 SCHMITT Vhigh=5.1 Trise=400n Vt=634m Vh=1m
A6 N026 N009 0 0 0 0 N018 0 SRFLOP Vhigh=5.1 Trise=20n Rout=30
A7 0 N025 N019 0 0 0 N026 0 OR Vhigh=5.1 Trise=20n Rout=30
A8 CT N034 0 0 0 0 N025 0 SCHMITT Vhigh=5.1 Trise=20n Vt=0 Vh=10m
E1 N033 0 N024 0 1
E2 N035 0 SS 0 1
R15 N033 N034 500
D16 N034 N035 IDEAL
R16 INV N027 1k
C2 NI N027 40p
R17 SYN 0 2k
R18 OSC N016 250
V2 N003 0 3.64
F1 0 CT V2 -1
D17 N003 RT IDEAL
R19 N016 0 3k
D18 N009 N016 D1_6
S5 0 DCH N009 0 LSW
D19 0 CT Z5_1
A9 N008 N010 0 0 0 0 N009 0 SRFLOP Vhigh=5.1 Ref=0.9 Trise=150n Tfall=250n
A10 N006 N007 0 0 0 0 N008 0 OR Vhigh=5.1 Trise=20n
A11 CT 0 0 0 0 0 N006 0 BUF Vhigh=5.1 Ref=3.2 Trise=20n
A12 CT 0 0 0 0 N010 0 0 BUF Vhigh=5.1 Ref=0.9 Trise=20n
A13 SYN 0 0 0 0 0 N007 0 BUF Vhigh=5.1 Ref=2 Trise=20n
.model NPN NPN
.model PNP PNP
.model HOUT SW(Ron=2.7 Roff=175k Vt=2.8 Vh=-2.1 Vser=1.1 Ilimit=0.6)
.model LOUT SW(Ron=10m Roff=175k Vt=2.8 Vh=-2.1 Vser=0 Ilimit=0.6)
.model IDEAL D(Ron=0 Roff=1G Vfwd=0)
.model D1_75 D(Ron=1.57 Roff=1G Vfwd=1.75)
.model D1_6 D(Ron=0 Roff=1G Vfwd=1.6)
.model Z5_1 D(Ron=1 Roff=1G Vrev=5.075)
.model Z40 D(Ron=0 Roff=175k Vrev=40)
.model Z5_6 D(Ron=1 Roff=1G Vrev=5.6)
.model D1_2 D(Ron=0 Roff=1G Vfwd=1.2)
.model LSW SW(Vt=2.55 Vh=-0.5 Ron=50 Roff=1meg Vser=0.3 Ilimit=50ma)
.ends sg3525a
*
*$
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.