2007-04-02 11:34 PM
2007-04-02 3:07 AM
Hi
Looking for some Assembly code for an ST7 29 Lite to transmit a few ASCII characters out an a single pin at 2400 Baud. I have looked at the one in the application notes but that ones enables and disables the interrupts, I would like to keep the interrupts going as I have some timing routines going that are called every 2mS I don’t mind generating an interrupt but I don’t want to disable them. Any pointers would be helpful. Re Brian2007-04-02 4:05 AM
Brian,
have a look at Application Note 1753 (http://www.st.com/stonline/books/pdf/docs/9986.pdf)2007-04-02 4:18 AM
Hi
I Have looked at this app but this is the code that turns the interrupt on and then off (RIM SIM). Looking for an alternative?2007-04-02 11:00 PM
Brian, some time ago I posted in this forum (see message: ''I must reload IMMEDIATELY LTCSR2: can I?'') the code for a software UART that sends and receives characters at 9600 baud in half-duplex style.
Even if this code is somewhat outdated (I made some improvements), I think it is a base to start from. Regards EtaPhi2007-04-02 11:34 PM
Thanks, I will have a look
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.