2007-04-04 12:05 AM
can not pull the pin stage from low to high when connect 2 ARM together?
2007-04-03 11:30 PM
1, connect 2 pins of 2 ARM together,
both pins configured as open drain, with external pull high resistors to 3.3V 2, initila at high state, then pull low by instruction but can not pull high anymore! any idea ?2007-04-04 12:05 AM
If the line stays low, then something is pulling it low. It can be either of the two ARMs. Double-check everything.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.