cancel
Showing results for 
Search instead for 
Did you mean: 

SCU_CLKCNTR - invalid values for STR91xFA?

michael
Associate II
Posted on April 14, 2008 at 10:30

SCU_CLKCNTR - invalid values for STR91xFA?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
michael
Associate II
Posted on May 17, 2011 at 09:52

Hello,

Could you please let me know if the register SCU_CLKCNTR can be configured to have an invalid value when the MCU is driven by a PLL (i.e. MCLKSEL = PLL)?

kais
Associate II
Posted on May 17, 2011 at 09:52

No.

michael
Associate II
Posted on May 17, 2011 at 09:52

hello eris,

do you mean that it cannot be configured invalid or that you cannot tell me (maybe because of the same reason...)?

One more thing: If I have an older revision of the chip (STR91xF revision B or D), then the only limitation is the speed of the flash (not faster than 48 MHz)?

Thanks in advance

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.