2017-02-26 1:17 AM
Hi
I`m new with the STM8S-Discovery and the STM8S105.I usually write my code in assembler so I get a deeper touch on the micros hardware.But I encountered an issue with the STVD tool.
When I`m entering the debug mode and push the RUN button I can seethe red LED next to the USB connector blinking. But the simple code does not work.The code should make the green LED blinking, but it doesn`t.I can`t see any error message or other info.But when I set the cursor on the first command(bset) of the code with SET PC(Debug menu)
and then select CONTINUE(Debug menu) the programm works. The green LED flashes correctlyuntil I stop the programm.I can read out the code with STVP, so the micro is flashed.
But the programm does not work after unplug and replug the USB connector.What I use:ST Visual Develop 4.3.10
Windows 10STM8S-Discovery (STM8S105C6)Debeug instrument: SWIM ST-LinkThe code looks like this:
--------------------------------------------------------stm8/segment 'rom'
start bset $5011,#0loop_forever ldw X,#$FFFFloop_delay nop decw X jrne loop_delay bcpl $500F,#0 jra loop_foreverend
--------------------------------------------------------Something wrong with my handling of the STVD or micro initialising?
Thanks for any helpIvan
2017-02-26 11:17 PM
Hello,
Did you setup you interrupt vector table correctly?
I am talking specifically about the reset vector: it should be pointing to your start label.
BR
Max
2017-02-28 5:02 AM
,
,
Hi Max
Thanks for reply. I used legacy ST62 micros until now. Like I said I write my code in assembler. With the ST62 I used a text file mycode.asm and compiled it with ast6.exe to get the mycode.hex which I sent to the ST62 with the programmer.
Set up the reset vector for ST62 usually looks like this
-----------------------------------------------------------------------------------------------------------
.org 0080h
start , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , ,
, , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , ,,main prog
.org 0ff0h
, , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , ,,some other vectors
.org 0ffch
jp , , ,nmi_int , , , , , , , , , , , , , , , , , , , , , ,,interrupt vector
jp , , ,start , , , , , , , , , , , , , , , , , , , , , , , , , , ,,reset vector pointed to the start of the program
.end
-----------------------------------------------------------------------------------------------------------
Now I use STVD and I`m not familiar with.
There is an automatic generated mapping.asm file which contains the info where to place the reset vector.
-----------------------------------------------------------------------------------------------------------
stm8/
,------------------------------------------------------
,
, SEGMENT MAPPING FILE AUTOMATICALLY GENERATED BY STVD,
, SHOULD NOT BE MANUALLY MODIFIED.,
, CHANGES WILL BE LOST WHEN FILE IS REGENERATED.,
,------------------------------------------------------,
♯ include 'mapping.inc'BYTES , The following addresses are 8 bits long
,
segment byte at ram0_segment_start-ram0_segment_end 'ram0'WORDS , The following addresses are 16 bits long
,
segment byte at ram1_segment_start-ram1_segment_end 'ram1'WORDS , The following addresses are 16 bits long
,
segment byte at stack_segment_start-stack_segment_end 'stack'WORDS , The following addresses are 16 bits long
,
segment byte at 4000-43FF 'eeprom'WORDS , The following addresses are 16 bits long
,
segment byte at 8080-FFFF 'rom'WORDS , The following addresses are 16 bits long
,
segment byte at 8000-807F 'vectit'END
-----------------------------------------------------------------------------------------------------------
So what I have to do now? Place
, , ,
, , ,segment , , ,
'vectit'
, , , , , , , , ,jp , , ,start
into my main program?
I found in the documentation INT as command to use instead of JP , but INT it`s not recognized as a valid comand by STVD.
Thanks for any help.
2017-02-28 10:50 PM
Can you understand C language?
STM8 has many examples and libraries written in C, but not much in assembly.
If you can understand C, it will probably simplify your life a lot...
This was not the case with ST6: its core was not good for C compiler efficiency and most development work was done in assembler.
If C is an option for you,
http://cosmicsoftware.com/download_stm8_free.php
as a version free of charge for STM8 and use thehttp://www.st.com/en/embedded-software/stsw-stm8069.html
either in your application or as example.Otherwise, look at this site
http://stm8sdiscovery.nano-age.co.uk/home
: it shows a very simple start using the assembler.Look at the Revenge of the blinking LED, it includes the interrupt vectors the way they should be for STM8
2017-03-01 5:08 AM
Thanks for the info. I used the vector table from 'the blinking led' page. It works now.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.