2021-10-19 3:36 AM
I have bought a STL8L Discovery kit and have installed the example for showing a clock: RTC using LSE - but it drift appx. 5 seconds per minute.
Seems like a simple 555 timer - or a cheap old analog clock - is more precise.
2021-10-19 4:25 AM
it looks as if you are not using the crystal-stabilized LSE, but by accident the RC-based LSI. Its frequency can vary between 26...56kHz, which corresponds to an RTC "error" of -20.6...+70.9%, i.e. about -12...+42s. Where did you find the sample program?
Regards
/Peter
2021-10-19 6:40 AM
From http://wwwst.com/stm8l -> STM8l15x_StdPeriph_Lib.zip\Project\STM8L15x_StdPeriph_Examples\RTC\
CLK_DeInit();
CLK_LSEConfig(CLK_LSE_ON); /* Enable LSE */
while (CLK_GetFlagStatus(CLK_FLAG_LSERDY) == RESET); /* Wait for LSE clock to be ready */
LSE_StabTime(); /* wait for 1 second for the LSE Stabilisation */
CLK_RTCClockConfig(CLK_RTCCLKSource_LSE, CLK_RTCCLKDiv_1); // Low Speed External
CLK_PeripheralClockConfig(CLK_Peripheral_RTC, ENABLE); // Enable RTC
RTC_DeInit();
RTC_StructInit(&rtc_init);
errStatus = RTC_Init(&rtc_init);
RTC_DateStructInit(&rtc_date);
errStatus = RTC_SetDate(RTC_Format_BIN, &rtc_date);
2021-10-19 7:54 AM
It looks like inspired by the example RTC_Calendar.
There are at least two possibilities: you either changed the clock assignment later, or the RTC automatically switched to LSI due to an error (see datasheet, section 3.5).
Regards
/Peter
2021-10-19 8:37 AM
Make sure you set the prescalers appropriately
RTC_InitStr.RTC_HourFormat = RTC_HourFormat_24;
RTC_InitStr.RTC_AsynchPrediv = 127;
RTC_InitStr.RTC_SynchPrediv = 255;
RTC_Init(&RTC_InitStr);
Suggest you read-back/dump the registers you currently run with to confirm the mode/settings, and that they are in fact correct and appropriate.
2021-10-19 8:40 AM
void init_rtc(void)
{
RTC_InitTypeDef RTC_InitStr;
RTC_TimeTypeDef RTC_TimeStr;
RTC_DateTypeDef RTC_DateStr;
#if 0
/* LSI */
CLK_RTCClockConfig(CLK_RTCCLKSource_LSI, CLK_RTCCLKDiv_1);
CLK_PeripheralClockConfig(CLK_Peripheral_RTC, ENABLE);
RTC_InitStr.RTC_HourFormat = RTC_HourFormat_24;
RTC_InitStr.RTC_AsynchPrediv = 0x7C;
RTC_InitStr.RTC_SynchPrediv = 0x012F;
RTC_Init(&RTC_InitStr);
#else
/* LSE */
CLK_LSEConfig(CLK_LSE_ON);
while (CLK_GetFlagStatus(CLK_FLAG_LSERDY) == RESET);
CLK_RTCClockConfig(CLK_RTCCLKSource_LSE, CLK_RTCCLKDiv_1);
CLK_PeripheralClockConfig(CLK_Peripheral_RTC, ENABLE);
RTC_InitStr.RTC_HourFormat = RTC_HourFormat_24;
RTC_InitStr.RTC_AsynchPrediv = 127;
RTC_InitStr.RTC_SynchPrediv = 255;
RTC_Init(&RTC_InitStr);
#endif
RTC_TimeStructInit(&RTC_TimeStr);
RTC_TimeStr.RTC_Hours = 00;
RTC_TimeStr.RTC_Minutes = 00;
RTC_TimeStr.RTC_Seconds = 00;
RTC_SetTime(RTC_Format_BIN, &RTC_TimeStr);
RTC_DateStructInit(&RTC_DateStr);
RTC_DateStr.RTC_WeekDay = RTC_Weekday_Tuesday;
RTC_DateStr.RTC_Date = 19;
RTC_DateStr.RTC_Month = RTC_Month_October;
RTC_DateStr.RTC_Year = 21;
RTC_SetDate(RTC_Format_BIN, &RTC_DateStr);
}
void rtc_get_time(char *buf)
{
RTC_TimeTypeDef RTC_TimeStr;
while (RTC_WaitForSynchro() != SUCCESS);
RTC_GetTime(RTC_Format_BIN, &RTC_TimeStr);
sprintf(buf, "%02d:%02d:%02d",
RTC_TimeStr.RTC_Hours & 0xff, RTC_TimeStr.RTC_Minutes & 0xff, RTC_TimeStr.RTC_Seconds & 0xff);
}
void rtc_get_date(char *buf)
{
RTC_DateTypeDef RTC_DateStr;
while (RTC_WaitForSynchro() != SUCCESS);
RTC_GetDate(RTC_Format_BIN, &RTC_DateStr);
sprintf(buf, "%04d-%02d-%02d",
(RTC_DateStr.RTC_Year & 0xff) + 2000, RTC_DateStr.RTC_Month & 0xff, RTC_DateStr.RTC_Date & 0xff);
}
2021-12-09 5:28 AM
Yes - thats my code!
2021-12-09 7:06 AM
Hi. Sorry - have been working on other projects - but I still haven't got this working.
Now I have copied the code from the "Discovery Board Demo", but I still can figure out how to change to LSE
I have tried to remove all function calls and defined types just to see if this was causing any problems. When debugging I get an error in line 22.
// Switch the clock to LSE
void init_LSE()
{
// CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_1);
// CLK_LSEConfig(CLK_LSE_ON);
// CLK_SYSCLKSourceConfig(CLK_SYSCLKSource_LSE); // Switch in LSE clock
// CLK_SYSCLKSourceSwitchCmd(ENABLE);
CLK->CKDIVR = (uint8_t)(0x00); // Set the System clock divider to 1
CLK->ECKCR &= (uint8_t)~0x04; // Reset LSEON bit
CLK->ECKCR &= (uint8_t)~0x20; // Reset LSEBYP bit
CLK->ECKCR |= (uint8_t)0x04; // Configure LSE
delay_ms(2000);
while (!((CLK->ECKCR)& 0x08)); // Wait flag LSE ready
CLK->SWR = (uint8_t)0x08; // Switch in LSE clock
CLK->SWCR |= (uint8_t)0x02; // Set SWEN bit - CLK_CKDIVR
while (((CLK->SWCR)& 0x01)==0x01);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.