2005-11-28 2:29 AM
Replacement or upgrade of ST62T42BQ6 Requested
2005-09-29 9:01 PM
Hello All,
I am looking for a replacement for ST62T42BQ6 chip. This is 64 pin PQFP64 package. Some of the salient requirements are OTP or cheapest varient, 8K ROM, 192 bytes RAM, 6 channel 8-bit ADC, TWO 8-bit timers with 7-bit prescaler and 40 x 4 LCD segment driving lines. If anybody is using any low-cost ST product which meets all of the above specs, please suggest. Thanks in advance.2005-09-30 12:17 AM
Replacement for ST62T42BQ6 is ST7 microcontrolers. According to your need you can select the appropriate one from the following link
http://mcd.rou.st.com/modules.php?name=mcu&file=familiesdocs&FAM=15#Datasheet You will find it easily rather with more accurate set of features except the LCD segment driving lines e.g . For that i will suggest you to go for software implemented LCD driver with full explanation in AN1048(available at link www.st.com/stonline/books/pdf/docs/6292.pdf ) It is very efficient in terms of speed and memory requirements.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.