2006-10-27 6:07 PM
Regarding- data transmission in zero crossing by ST7538 (important)
2006-10-27 6:07 PM
Sir,
I am using Synchronous mode in communication by ST7538. So every bit is transmitted by the CLR/T clock. Now my task is to transmit data ie 1 bit in zero crossing time of AC cycle. Since modem has the facility to generate zero crossing pulse, i have given proper hardare to generate zero crossing pulse.now i am getting zero crossing output ZCOUT. i did enable the 11th bit (Command Write) for zero crossing sysnchronisation. * Is it possible to send 1 bit as frequency? also Is it possible to detect in Reciever side? * Is preamble transmission compulsary? because every time i want to transmit only 1 bit of my data. * Is CLR/T necessary to transmit data? * I want to transmit a bit as such transmit a bit in zero crossing then stop and then again transmit next bit in next zero crossing. * Also send me other possiblities.(asynchronous method or any other chips) * Also is there any 5 msec period cycle - CLR/T clock which synchronise with ZCOUT clock posedge or negative edge.(Any other IC) I EXPECT YOUR REPLY VERY SOON, THANK U SARAVANAN.V.AWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.