2018-08-13 11:05 PM
Hello Sir/Madam,
Greetings!!!!!
This is Akshay pathak working as a Embedded Hardware Engineer in Teksun Microsys Pvt Ltd.
I have some query regarding the analog switch IC part No. STG3693.
We want to evaluate basic audio application by using of analog switch IC (Part no: STG3693) which have an R(ON) resistance 4 ohm.In that, we want to disturb the audio signal of headphone speakers as well as a mic. so we implement this analog switch between headphone and mobile.
So my point is if this part is suitable for our application or not and if not then suggest us correct part which is suitable for our application.
Kindly let me know if you have any query or need more information for the same.
Thanks,
Akshay Pathak.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.