2018-08-13 10:02 AM
Hi
I'm using L9825 in one of my applications and have couple of questions just to make sure I get it right:
1- I have Vcc=3.3v and Reset line pulled high. Is that ok?
2- my understanding is that NON1 and NON2 can be used to directly drive OUT1 and OUT2 independently of SPI interface; So after setting NON1 and NON2 to digital low/high, do I need to use the NCS line at all? anything else that I should consider?
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.